{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number of the USB cable used to connect a PC to a drive or soft start when using SoMove?
Issue:
Cable part number to connect a PC to a drive or soft start when using SoMove or Powersuite?

Product Line:
ATV Altivar Drive ATS Altistart Soft starter

Environment:
All current products

Resolution:
TCSMCNAM3M002P:  This cable is a USB to RS485 interface cable to be used with SoMove and Powersuite.
The cable connects to the the ModBus port on the drive and a USB port on a PC.

cable image
Note: If using this cable with SoMove, then the SoMove software must be installed on your PC prior to plugging this cable into the USB port on the PC. The driver for this cable is now included in the core SoMove software. And it's important that your PC uses this driver as opposed to a driver that Windows would install automatically.

Schneider Electric Egypt and North East Africa