{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the reference for the mechanical interlock for 1 out of 3 ATS system with MCCBs ?

Mechanical interlocks for 1 out of 3 MCCB systems are not available.
The only alternative solution is locking manually using key locks. You can find the catalogue page attached. Selection of the type of lock depends on the type of handle.

Schneider Electric Egypt and North East Africa

Attachment(s)

NSX400-630 locks.pdfNSX400-630 locks.pdf [264.55 KB]
NSX 100-250 locks.pdfNSX 100-250 locks.pdf [184.39 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: