{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Uniflair BACnet (Building Automation and Control Networks)


Issue:
This document describes the operation of the Uniflair BACnet (Building Automation and Control Networks).

Product line:
Uniflair

Environment:
All Models and Serial Numbers

Cause:
Install

Resolution:

Units with RE485 serial boards

Serial card Gateway

All the units must be fitted with a RS485 card, trough that they are connected to the RS485 serial cable. On one side there will be the 120 ohm resistor, on the other, the gateway which will translate the variables from Uniflair language, to LON language.

To realize a local net to be connected to a BMS with protocol BACnet, it’s necessary:

• gateway LBM every 8 units; (not necessary with pCOnet - pCOWeb)

• 1 RS485 serial card for every controller;

• 120Ω resistor;

• PC for the gateway configuration

BACnet is a supervisory system created from AHRAE:

“American society of Heating, refrigerating and Air conditioning Engineers”

These are the ways how the information under BACnet can be sent to Uniflair controllers:


  BACnet IP/Ethernet
BACnet IP/Ethernet

RS485 PCONET pCOnet:  RS485

Gateway Gateway

Carel :

  1. Protocol Carel
  2. Connection RS485 or RS422
  3. Max 8 units
  4. No software modification needed

BACnet :

  1. BACnet PTP
  2. Connection RS232

Schneider Electric Egypt and North East Africa