Search FAQs
Does the ATV312 braking resistors come with temperature thermal protection?
Issue:
Thermal protection temperature switch included in braking resistor VW3A7723
Product Line:
Altivar 312; ATV312
Environment:
All models, all serial numbers
Cause:
The documentation that comes with the resistor does not indicate.
Resolution:
Braking resistors VW3A7723 to VW3A7725 do not have thermal protection temperature switches. Braking resistors VW3A7701 to VW3A7705 has thermal protection temperature switches. The tripping temperature is 120 deg. C. Max voltage - current AC = 250V ~ 1 A DC = 24V ~ 0.1 A
Thermal protection temperature switch included in braking resistor VW3A7723
Product Line:
Altivar 312; ATV312
Environment:
All models, all serial numbers
Cause:
The documentation that comes with the resistor does not indicate.
Resolution:
Braking resistors VW3A7723 to VW3A7725 do not have thermal protection temperature switches. Braking resistors VW3A7701 to VW3A7705 has thermal protection temperature switches. The tripping temperature is 120 deg. C. Max voltage - current AC = 250V ~ 1 A DC = 24V ~ 0.1 A
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: