{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Altivar 212 drive provide input phase loss detection?

Article available in these languages: Japanese

Issue:
Input Phase Loss Detectoin on Altivar 212

Product line:
Altivar 212

Environment:
All models, all serial numbers

Cause:
Phase loss protection

Resolution:
Yes, the Altivar 212 monitors both the input and output phases so it will fault.  The fault code for input phase lose is EPHI.  The fault code for output phase loss is EPHO.

Schneider Electric Egypt and North East Africa