Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How do I update the “Date of last Battery Replacement” seen in NMC card GUI?
Issue:
How do I update the “Date of last Battery Replacement” seen in NMC card GUI?
 
Product line:

Smart-UPS VT, Galaxy 3500, Symmetra PX1
 
Environment:
All models, all serial numbers
 
Cause:
The system does not automatically update battery age / replacement information, it must be manually changed whenever all of the batteries are replaced.
 
Resolution:

Log into the NMC web interface click on the UPS tab then under the Configuration section is the option for General, select General and you will see the options for “last battery replacement”
 
1
 
And
 
2
 
 Update when all batteries have been replaced.
 Note, This only applies to units running FW 5x or lower
 
 
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: