{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

EcoAisle versus HACS

Issue:
What are the key features of the new EcoAisle system that will be replacing the traditional HACS.

Product line:
EcoAisle.

Environment:
Containment Systems.

Cause:
Install.

Resolution:

•      Active Flow Control  - Right sizes cooling airflow while providing visibility to effective cooling to critical IT equipment.

•      Flexibility - Support for varying aisle widths, rack heights,  rack depths, and single rows. Supports hot aisle containment or cold aisle containment.

•      Fire Safe System  - Alerts personnel and drops ceiling panels based on temperature (per UL723S standards) or field supplied smoke detector to enable fire suppression system in the room to extinguish the fire.

•      EcoLEDgy Driven Lighting- Integrated High Efficiency LED lighting with on/off motion sensors

•      Safe Slide Doors - Emergency break away sliding door enables quick exit  in the event of an emergency

•      Air Return System - Centralized hot air return system for room and external air handling systems minimize obstruction of lighting into the ducted aisle and provide cable access from within the contained aisle

•      Over Aisle Access – Tooless removal of individual panels to allow access above the aisle for cabling and maintenance.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: