{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is meant by thermal current rating (Ith) for Contactor "D" or "F" type ?

It means the rated current that this contactor can switch for Load category AC1 (thermal loads),

Example: LC1D09 is 9 A on AC3 and its thermal current (Ith = 20 to 25 A) (this means it can switch up to 20 or 25 A for loads of AC1

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: