Search FAQs
Can the NetShelter CX integral PDU be replaced, or can another be added if a dual power input is required for redundancy? Which PDU comes in the CX?
Issue:
Need an additional or replacement PDU in the NetShelter CX.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Additional PDU or replacement necessary
Resolution:
Yes, the PDU can be replaced or others can be added.
The original PDU included with the cabinet is the APC part number AP9568 for EMEA cabinets (50Hz), and AP9567 for NEMA cabinets (60Hz).
Need an additional or replacement PDU in the NetShelter CX.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Additional PDU or replacement necessary
Resolution:
Yes, the PDU can be replaced or others can be added.
The original PDU included with the cabinet is the APC part number AP9568 for EMEA cabinets (50Hz), and AP9567 for NEMA cabinets (60Hz).
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: