{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will the NetShelter CX fit through standard doors?
Issue:
Will the CX fit through a standard door opening?

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Need to ensure the NetShelter CX will fit up the stairs, into the elevator or through a doorway.

Resolution:
All the units, including the 38U, are designed to go through a standard doorway. They measure 750 mm /29.5” wide x max 1950mm/76.7” tall.

Schneider Electric Egypt and North East Africa