Issue:
What is the error code dCb on the Altivar Drive's display.
What is the error code dCb on the Altivar Drive's display.
Product line:
Altivar drive families: ATV12, ATV28, ATV312, ATV32, ATV61, ATV71.
Altivar drive families: ATV12, ATV28, ATV312, ATV32, ATV61, ATV71.
Environment:
All models, all serial numbers.
All models, all serial numbers.
Cause:
DC Injection Braking.
DC Injection Braking.
Resolution:
This is a normal drive state. It is indicating the drive is injecting DC current into the motor to slow the motor down. This typically appears on deceleration or at the end of the deceleration ramp. On some drives, DC Injection can be turned on using a Logic Input.
This is a normal drive state. It is indicating the drive is injecting DC current into the motor to slow the motor down. This typically appears on deceleration or at the end of the deceleration ramp. On some drives, DC Injection can be turned on using a Logic Input.
Released for:Schneider Electric Egypt and North East Africa