{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the hole size of the padlock provision for a GV2P starter?
Issue:
Padlock hole diameter on GV2P

Product Line:
GV2 Manual Motor Protectors

Environment:
All GV2P, rotary handle.

Cause:
n/a

Resolution:
There are provisions for one padlock only, the hole size is approximately 6mm.  You can add a GV2V03 padlock attachment that will allow up to 6 padlocks for Lock out Tag out applications.

Schneider Electric Egypt and North East Africa