This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Unity V7.0 is compatible with windows 7 32 and 64 bit
On Windows 7 64bits System, installation of Windows 7 Service Pack 1 (SP1) is mandatory in order to use Unity Pro V7.0
On Windows 7 64bits System, installation of Windows 7 Service Pack 1 (SP1) is mandatory in order to use Unity Pro V7.0
Released for: Schneider Electric Egypt and North East Africa