Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why the RCCB is only 2P and 4P ? & Why the Vigi module is 3P ?
The RCCB must see the live phases and the neutral.

When we install the earth leakage module with the incoming breaker, it will disconnect the whole system when an earth leakage occur at any MCB.

For that the RCCB is 2P (1P+N) and 4P (3P + N)

Sometimes, the system's 220V is line to line, so we will have two live poles. To protect them against earth leakage, we will need 3P.
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: