Issue:
Store and transfer program files using VW3A1101 keypad.
Product Line:
Altivar ATV312
Environment:
All models, all serial numbers.
Cause:
A duplicate program is to be used on multiple drives.
Resolution:
No. Although the VW3A1101 is compatible with ATV312, it cannot be used to transfer a program file from one ATV312 to another. A Multi-Loader or Simple Loader tool or SoMove software can be used to transfer files.
Store and transfer program files using VW3A1101 keypad.
Product Line:
Altivar ATV312
Environment:
All models, all serial numbers.
Cause:
A duplicate program is to be used on multiple drives.
Resolution:
No. Although the VW3A1101 is compatible with ATV312, it cannot be used to transfer a program file from one ATV312 to another. A Multi-Loader or Simple Loader tool or SoMove software can be used to transfer files.
Released for:Schneider Electric Egypt and North East Africa