{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How does one set up the ATV61/71 keypad VW3A1101 to display more than one parameter?
Issue:
ATV61/71 keypad VW3A1101 set up to display more than one parameter.

Product line:

Altivar 61 and 71

Environment:
All models, all serial numbers:

Cause:
One parameter is the default.

Resolution:
From the main menu go to menu 6 [Monitoring Config] then enter
Select 6.2 [MONITOR SCREEN TYPE].
If "Digital value type" is "Digital" only two parameters can be selected.
If "Digital value type" is "Bar graph" only two parameters can be selected.
If "Digital value type" is "List" then five parameters can be selected.
Go to "PARAMETER SELECTION".  Select the check box beside the parameters you want to display.

Schneider Electric Egypt and North East Africa