{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How is standard basic programming performed on an ATS48?

Article available in these languages: Spanish

Issue:
How is an ATS48 set up for basic programming?

Product line:
Altistart 48

Environment:
All models, all serial numbers

Cause:
Basic programming set up for the ATS48 soft starters.

Resolution:
SET menu:
IN= FLA motor amps
ACC= acceleration
STY= type of stop (f=freewheel, d=ramp stop, b=intel braking)
DEC= deceleration [only appears if Sty= d (ramp stop)]
ILT=current limit 400%  or 4X your motor current is default value.

DRC menu:
CLP= Off (Torque Control).  This is important if the ACC/DEC times have to be followed exactly.

Refer to the ATS48 User Manual for any further details. 

The following video demonstrates this initial setup procedure:

 
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.