{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATV61 have an EMC filter?
Issue:
is EMC Filter built-in on ATV61?

Product Line:
Altivar 61

Environment:
All models except the ATV61H...M3X series.

Cause:
None

Resolution:
Altivar 61 drives, except for the ATV61H...M3X, have built-in radio interference
input filters to meet the EMC standard for variable speed electrical power drive
“products” IEC/EN 61800-3, edition 2, category C2 or C3 in environment 1 or 2 and
to comply with the European directive on EMC (electromagnetic compatibility).

Schneider Electric Egypt and North East Africa