{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Available Input Contact and Output Relay events on the AP9613 Dry Contact I/O SmartSlot Card


Issue

Which events can be triggered from an either an input contact or output relay on the AP9613 Dry Contact Relay I/O SmartSlot Card?


Product Line
  • UPS Device Management
    • AP9613 Dry Contact I/O SmartSlot Card
    • AP9335T/TH Environmental Sensors
    • AP9810 Dry Contact I/O Accessory Dongle

Environment
  • All firmware versions
  • All serial numbers

Cause

General information - if a user is interested in which events can be mapped to an input contact or output relay on the AP9613, refer to the list below.  Legacy Configuration options (those available with the older AP9610 SmartSlotCard) are available via dip switch configuration (outlined in the user's guide) or also as a template in the configuration utility the AP9613 offers.

If you would like to customize which inputs or outputs map to which commands and/or relay numbers, please refer to the user's guide for the AP9613 in using the "Custom" dip switch configuration in order to utilize the Dry Contact I/O SmartSlot Card Configuration Utility to do the customization.


Resolution

The available targets on the standalone AP9613 for input contacts include:

  • UPS
  • UPS Outlet Group 1*
  • UPS Outlet Group 2*
  • UPS Outlet Group 3*
  • Output Relay 1
  • Output Relay 2
  • Output Relay 3
  • Output Relay 4
  • Output Relay 5
  • Output Relay 6
  • UIO Port 1 Output Relay (if optional AP9810 is connected)
  • UIO Port 2 Output Relay (if optional AP9810 is connected)

If you choose the UPS or an Outlet Group as the target, the following (control) Actions are available:

  • On
  • On With Delay
  • Off
  • Off Gracefully
  • Shutdown
  • Shutdown with Delay (With outlet groups only)
  • Reboot
  • Reboot Gracefully
  • Self Test (Not available with outlet group target)
  • Bypass* (Not available with outlet group target)


The available events on the standalone AP9613 for output relays include:


As an added option and for expansion, the AP9613 has (2) Universal I/O ports that support the following accessories:
  • AP9335T or AP9335TH Temperature or Temperature and Humidity Sensors
  • AP9810 Dry Contact I/O Accessory

With the optional AP9335T or AP9335TH Environmental Sensors, the following alarms can be configured:

  • Temperature Above Maximum
  • Temperature Below Minimum
  • Humidity Above Maximum
  • Humidity Below Minimum

These environmental alarms as well as the inputs from the optional AP9810 Dry Contact I/O Accessory Dongle can then be mapped to one of the following targets:

  • UPS
  • UPS Outlet Group 1*
  • UPS Outlet Group 2*
  • UPS Outlet Group 3*
  • Output Relay 1
  • Output Relay 2
  • Output Relay 3
  • Output Relay 4
  • Output Relay 5
  • Output Relay 6
  • UIO Port 1 Output Relay (if optional AP9810 is connected)
  • UIO Port 2 Output Relay (if optional AP9810 is connected)

If you choose the UPS or an Outlet Group as the target, the following (control) Actions are available:

  • On
  • On With Delay
  • Off
  • Off Gracefully
  • Shutdown
  • Shutdown with Delay (With outlet groups only)
  • Reboot
  • Reboot Gracefully
  • Self Test (Not available with outlet group target)
  • Bypass* (Not available with outlet group target)

If you choose an Output Relay as a target, the following Actions are available:
  • Abnormal
  • Normal



note exclamation*Not available on all devices. Please verify that your UPS supports this function.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: