Issue:
Replacement power board part number for ATV61 drives.
Product Line:
ATV61, Altivar 61
Environment:
It is required to check the Serial number of the drive before ordering the Power Board.
If the 8th digit in the serial number is 2, the drive was built using Fuji IGBT's instead of the standard Mitsubishi IGBT's. A drive with Fuji IGBT's requires a modified version of the Power board (VX5A1HC1113F). IGBT, measuring board and gate driver board parts also will have an F at the end.
Cause:
N/A
Resolution:
Released for:Schneider Electric Egypt and North East Africa