Issue:
Needs a replacement part number for an ATV11 drive.
Product Line:
Altivar 11
Environment:
All models and serial numbers
Cause:
Determine the replacement for an ATV11 drive.
Resolution:
The recommended replacement for the ATV11 is the ATV12. Select the ATV12 based on the motor horsepower, rated motor voltage and supply voltage (single or three phase).
Needs a replacement part number for an ATV11 drive.
Product Line:
Altivar 11
Environment:
All models and serial numbers
Cause:
Determine the replacement for an ATV11 drive.
Resolution:
The recommended replacement for the ATV11 is the ATV12. Select the ATV12 based on the motor horsepower, rated motor voltage and supply voltage (single or three phase).
Released for: Schneider Electric Egypt and North East Africa