Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between Plug-in and Fixed NSX Circuit Breaker ?
The plug-in version makes it possible to:
  • Extract and/or rapidly replace the circuit breaker without having to touch the connections on the base
  • Allow for the addition of future circuits by installing bases that will be equipped with a circuit breaker at a later date
  • Isolate the power circuits when the device is mounted on or through a panel. It acts as a barrier for the connections of the plug-in base. Insulation is made complete bythe mandatory short terminal shields on the device.The degrees of protection are: circuit breaker plugged in = IP4
    circuit breaker removed = IP2
    circuit breaker removed,base equipped with shutters = IP4.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: