{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Can we perform Automatic Transfer switch (1out of 2) using withdrawable version from MCCB of type NSX ?

- The ATS (Automatic transfer switch 1 out of 2) using the NSX MCCB can only be performed using:

1- Fixed MCCB NSX
2- plug in MCCB NSX

Attached here Catalog pages illustrate this info as well as connections for NSX ATS

Schneider Electric Egypt and North East Africa

Attachment(s)

Source Changeover.pdfSource Changeover.pdf [361.89 KB]
100 TO 630 NSX Source Changeover Assembly 00999531A 01.pdf100 TO 630 NSX Source Changeover Assembly 00999531A 01.pdf [2.65 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: