Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the methods of Mechanical interlocks used with MCCB NSX ?
 the methods of Mechanical interlocks used with MCCB NSX  can be one of the following:

1- Mechanical interlock on the frame of MCCB NSX for toggle operated breakers

2- Mechanical interlock on the frame of MCCB for rotary handle operated breakers

3- Mechanical interlock built in mounting plate for two fixed or plug in MCCB NSX (used for ATS 1 out of 2) 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: