{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Does the ACSC automatically restart after a high head pressure alarm?
Issue:
Does the ACSC automatically restart after a high head pressure alarm?

Product line:
ACSC100, ACSC101

Environment:
InRow Cooling

Cause:

Resolution:
Yes, if the ACSC sees the HP switch open, it will switch into idle mode and then attempt to restart after a 2 minute delay. If the unit had the HP switch open three times within 30 minutes, the ACSC will go into Persistent High Discharge alarm and will lock out the compressor. This alarm will need to be reset manually.

Schneider Electric Egypt and North East Africa