This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
What is capacity regulation on an ACRD?
Product line:
ACRD100, ACRD101, ACRD200, ACRD201
Environment:
Data Center Cooling
Cause:
Resolution:
Capacity regulation is a method of controlling the capacity of the InRow ACRD unit. This is achieved using an electronic Hot Gas Bypass Valve (HGBV) which allows the unit to operate at low load conditions down to 2.5 KW without compressor recycling.