This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
EasyPact circuit breaker can be supplied from either the top or the bottom (reverse feeding) without any reduction in performance for earth leakage circuit breakers, reverse feeding is possible only up to 240 V AC.
This capability facilitates connection when installed in a switchboard.