{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the function of protection modules of thr Plug in Relays ?

Whenever an inductive load is de-energised (coil of a relay or of a contactor), an overvoltage appears at its terminals. This voltage peak can reach several thousand volts and a frequency of several MHz.
It is likely to disturb the operation of automation systems which contain electronic devices.
Protection modules are used to reduce the voltage peak on de-energisation and they therefore limit the energy of interference signals to a level that will not disturb surrounding coils and electronic devices.

The function of each of these modules is indicated below :

Schneider Electric Egypt and North East Africa