This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
A limit switch complies to this specification when all the closed contact elements of the switch can be changed, with certainty, to the open position (no flexible link between the moving contacts and the operator of the switch, to which an actuating force is applied)
This enables the limitswitch to be used for safety applications as it esures the opening of the closed contact even if the contacts are welded .
This feature is indicated by the symbolin the limit switches catalog .
Released for: Schneider Electric Egypt and North East Africa