{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the SIS Gateway and is there any technical data for it?

Substation Controller (SIS Gateway)

The database concentrator of industrial networks

Basic functionalities:

  • Protocol conversion: bi-directional interface between some serial type networks and an Ethernet network
  • Acquisition  of information from IED's (up to 128 IED's)
  • Database concentration: each TCP client (SCADA, PLC's, DCS, ...) connected to the gateway has it's own database to optimize it's needs.
  • Duplication of time tagged events from IED's for each TCP subscriber.
  • Availability of communication linked to Linux base and management of a redundant communication with the IED's and TCP Clients
  • Time tagging of information from IED's which does not offer this functionality.
  • Transparent mode with frame priority access from TCP client
  • File configuration tool for Gateway setting
  • Serial channels are independent and used in parallel (up to 16 serial ports)
  • Integrated web server, enabling access to communication diagnostics, internal variable status.
  • Simulated mode: RTU, Internal Database modification, Avalanche, control ...

New generation:

SISGW first generation has been provided for more than 20 years between 2001 and 2022.

In 2022 Schneider developed a new generation of SISGW with new components and latest Linux version. This SISGW-NG is available since 2023 and is a full plug&play retrofit solution to existing SISGW: same size, same functionalities, same configuration. Using the new generation, the replacement of a SISGW to a SISGW-NG is transparent for IEDs and TCP Client.


For more information : see attached file .
Contact: Patrice Eyraud or Lionel Cotton
patrice.eyraud@se.com / lionel.cotton@se.com

Schneider Electric Egypt and North East Africa

Attachment(s)
PRES_SIS GatewayA4_VE_EN.pdf [330.08 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.