Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between earth fault protection and earth leakage protection?
Earth fault protection is intended to protect equipment when an insulation fault occurs, for instance a direct contact between a life conductor and earth. In such a situation, great fault currents will flow back to the transformer through its neutral point when its connected to earth (we can use SGR + MDGF module for detection).
This is not the case of earth leakage protection, where faulty currents are generally much lower and the protection is dedicated, for example, to avoid hazards to human beings or animals.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: