Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
In VSD coordination tables in catalog, Why the line contactor has current rating less than the line current of the drive ?
The combination given in the catalog are tested and validated for type-2 coordinatio .

The contactor used with VFD will be considered as AC-1 duty application, hence the continuous current rating of will be greater than the continous curent of the VSD

For Example, The contactor LC1D09 is AC-3 duty = 9Amps & AC-1 Duty = 25 Amps.so it can be used with VSD with continous current up to 25 A
 

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more