Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why isolation transformer is required for earth leakage relays (RH99 ) with auxiliary supply less than 48V?
We need a transformer with 2 winding to warranty the isolation with upstream
as the Isolation transformer is used to transfer electrical power from a source of alternating current (AC) power to some equipment or device while isolating the powered device from the power source, usually for safety. Isolation transformers provide galvanic isolation and are used to protect against electric shock, to suppress electrical noise in sensitive devices, or to transfer power between two circuits which must not be connected. Isolation transformers block transmission of the DC component in signals from one circuit to the other, but allow AC components in signals to pass.
Suitably designed isolation transformers block interference caused by ground loops. Isolation transformers with electrostatic shields are used for power supplies for sensitive equipment such as computers or laboratory instruments
as the Isolation transformer is used to transfer electrical power from a source of alternating current (AC) power to some equipment or device while isolating the powered device from the power source, usually for safety. Isolation transformers provide galvanic isolation and are used to protect against electric shock, to suppress electrical noise in sensitive devices, or to transfer power between two circuits which must not be connected. Isolation transformers block transmission of the DC component in signals from one circuit to the other, but allow AC components in signals to pass.
Suitably designed isolation transformers block interference caused by ground loops. Isolation transformers with electrostatic shields are used for power supplies for sensitive equipment such as computers or laboratory instruments
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: