{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which S-flex 212 drives have fusible disconnect or circuit breaker?

Issue:
Customer needs to know which S-flex 212 drives have a fusible disconnect or circuit breaker?

Product Line:
ATV212 S-Flex

Environment:
ATV212 (1 hp-100 hp S-Flex)

Cause:
Which enclosed units have fuses and which come with circuit breakers?

Resolution:
All of the S-Flex drives will have circuit breakers for short circuit protection except the 460VAC 75HP, 100HP SFD212RG4 and SFD212SG4.  These two will have a fusible disconnect.

Note: All of the 460VAC units will have power fuses and circuit breakers except the 75HP and 100HP that will not have the circuit breaker but only fuses.

Schneider Electric Egypt and North East Africa