{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which drives allow a program file to be transferred from the Multi-Loader without being powered up?

Issue:
What Drives can transfer a program file from Multi-Loader without it being powered up?

Product Line:
VW3A8121 Multiloader tool

Resolution:
ATV12, ATV32, and ATV320 drives will accept a file transfer from the VW3A8121 Multi-Loader while the VFD is unpowered, still in the box.
The ATS22, ATS48, ATV212, ATV61 and ATV71 all have to be powered up before the Multi-Loader can transfer the program file.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa