{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum duty cycle of the braking transistor of the ATV32 series drives?
Issue:
Does Schneider Electric list the ATV32 maximum duty cycle of the braking transistor?

Product Line:
Altivar 32

Environment:
All models, All serial numbers.

Cause:
Application requiring a braking transistor's continuous use

Resolution:
The braking transistor in the ATV32 series drives is designed to handle Nominal motor power continuously and 150% of nominal motor power for 60 seconds.
An appropriately sized braking resistor must be used that is also capable of handling the required duty cycle.

Schneider Electric Egypt and North East Africa