{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is PID set up on ATV12 drives?
Issue:
ATV12 PID loop set up.

Product Line:
Altivar ATV12

Resolution:
Yes, PID regulator settings can be found under the FuN menu.
[Conf] -> [Full] -> [Fun]
At 'PId' press Enter
PIF= PID feedback assignment Set to AI1 (Choice not possible if Fr1 is set to AI1)
PII= Activation of internal PID reference (Yes or No)
rP1= internal PID reference  (0 to 100%)
rPL= PID min value reference (0 to 100%)
rPH= PID max value reference (0 to 100%)

For further details, please see the ATV12 User Manual starting on page 72.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa