Product Line
SEPAM Relays
SFT2841
Environment
SEPAM SFT2841 software installation
Resolution
The serial numbers to use while installing the software are:
- For SFT2841 versions 11 and above: 0647740-08
- For SFT2841 versions below 11: 8888888-06
undefined undefined
{}
Product Line
SEPAM Relays
SFT2841
Environment
SEPAM SFT2841 software installation
Resolution
The serial numbers to use while installing the software are:
- For SFT2841 versions 11 and above: 0647740-08
- For SFT2841 versions below 11: 8888888-06