{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do the HV circuit breakers and contactors work at 60 Hz ?

The HV circuit breakers and contactors work as well as 50 Hz and 60 Hz.
IEC 62271 is applicable to a.c. circuit-breakers designed for indoor or outdoor installation and
for operation at frequencies of 50 Hz and 60 Hz on systems having voltages above 1 000 V.

Schneider Electric Egypt and North East Africa

Attachment(s)

1. using at frequency 60Hz.ppt1. using at frequency 60Hz.ppt [288 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: