{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to save of alarm message histories?

Basic principle
For Sepam series 20 and series 40,



The saving of alarm message histories can only be done by a remote monitoring and control system since this is the only effective means of saving in a substation that includes several Sepam devices. The devices are connected in a Modbus network to the remote monitoring and control system.



However, there is a simple but effective way to save individual Sepam histories, if the customer accepts to connect locally to the Sepam with a PC.

The procedure is described below:



Sepam series 20

The only possibility consists of saving a screen copy as follows:

- SFT2841 is connected to the Sepam

- select the diagnosis icon, history tab

- save the screen by pressing ALT + Print Screen

- paste in a Word filing by pressing CTRL+V

- name and save the file


Legacy KB System (APS) Data: RESL166597 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 20

Schneider Electric Egypt and North East Africa