{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How is Sepam 1000+ connected to existing core balance CTs?

The core balance CT interface ACE990 is used to match the measurement of an existing MV core balance CT with ratio 1/n (50=< n =< 1500) with that interface connected to the residual current input of Sepam 1000+.

Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166633 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 40, ACE 9XX, Sepam series 20

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.