{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why are there some communication failures between PC (SFT2841) and Sepam 1000+?

For security reasons, the communication supply (at the front plate) of Sepam 1000+ is totally isolated from the product internal power supply.
The communication supply is done by the PC serial port.

In some cases, when the serial port power supply is weak, and due to the components tolerances, a communication failure could occur.

If this kind of failure occurs again, it is advisable to use another PC.

Improvement of the communication level efficiency is available with the new Sepam base board (universal power supply from 24 to 250V).

This problem does not concern Sepam 1000+ series 40

Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166846 V2.0, Originally authored by FrKr on 06/18/2008, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 20

Schneider Electric Egypt and North East Africa