Search FAQs
Could you clarify the meaning of "PUP" in the Comtrade file of SFT2826?
PUP is the "pick-up" of the fault. Often people mistake "PUP" as the pickup of disturbance recording, but this is incorrect because the disturbance recording is often configured with pre-trig cycles that are used to view the recording before the actual disturbance. "PUP" relates to the instantanious pickup of a protection function, input, control logic or any other condition that sends a tripping order to the CB. This information is very usefull when analyzing a comtrade file because it helps find the origin of a sepam trip and system shutdown.
Re-published to revised security level: 20 June 2008 by DRM
Applies to: SFT2826
Internal PMO/PMC Support
All content © 1992-2007 Schneider Electric
AEDL3
Legacy KB System (APS) Data: RESL188980 V2.0, Originally authored by KBAdPM on 11/08/2007, Last Edited by DaMi on 06/21/2008
Related ranges: SFT 2826 (OPG display)