{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the length (in ms) of impulse in pulsed mode of output relays (O1, O2, O3) in Sepam 20?

Goals and Symptoms

What is the length (in ms) of an impulse in pulsed mode of output relays (O1, O2, O3) in Sepam 20.

Causes and Fixes

On Sepam 20, the time duration of a pulse of an output relay in pulsed mode is 14 ms, which is the duration of an internal cycle of Sepam.
It's the same on Sepam 40.

On Sepam 80 the basic duration is the same but you can adjust if needed the duration of the pulse with control logic.

AEDL3


Legacy KB System (APS) Data: RESL201041 V1.0, Originally authored by KBAdPM on 01/20/2010, Last Edited by KBAdPM on 01/20/2010
Related ranges: Sepam series 20

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: