{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What can CET850 configure for the IEC61850 protocol for SEPAM?

Issue
What is the CET850 used for?

Product Line
CET850

Resolution
CET850 can be used to:
1. Create an IEC61850 configuration using an ICD file or add a Sepam to an existing configuration.
2. Edit an existing CID or SCD file to modify its contents:
a. Add or remove a Sepam
b. Display the configuration
c. Modify communication parameter values
d. Optimize configuration by creating or modifying the dataset and report control block.
Note: The CID or SCD file may come from SFT2841
3. Generate a CID file for storing the configuration of one device which can then be downloaded to the Sepam or ECI850 using SFT2841 or by FTP with a standard internet browser.
4. Generate an SCD file for storing the configuration of an IEC61850 system which may then be used by other IEC61850 configuration tools.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: