Search FAQs
MiCOM S1 Studio Error: Data model file is not installed
Issue
Error message: "Data model file is not installed"
Product Line
MiCOM relays
Environment
MiCOM S1 Studio
Cause
This error will populate in MiCOM S1 Studio if one is attempting to connect to a MiCOM relay without the data model being installed.
Resolution
Refer to FA221295 for detailed instructions on how to add the data models.
The latest version of Easergy Studio (MiCOM S1 Studio) can be found here: https://www.se.com/ww/en/product-range-download/61035-micom-s1-studio
Legacy KB System (APS) Data: RESL210416 V1.0, Originally authored by DaFr on 01/24/2013, Last Edited by DaFr on 01/24/2013
Related ranges: MiCOM S1 Studio
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: