{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What type of batteries are used with the ADVC 2 controller?

Product Line
ADVC 2

Resolution
The batteries used for backup power, for the ADVC 2 controllers, are standard sealed lead acid batteries.  Any battery meeting the amp hour ratings may be used as a substitute.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.