Search FAQs
What is the accuracy of the Timers in ProWorx32?
Issue:
Accuracy of the Timers in ProWorx32
Product Line:
ProWorx32
Resolution:
The accuracy of a timer is +/- one incremental value or the scan time which ever is greater. So a T.01 timer has an accuracy of +/- 0.01 seconds provided that the scan time is less than 0.01 seconds.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: