Search FAQs
What is the replacement part number of the PCI SA85 Modbus Plus card P/N 416NHM3003x?
Issue:
Replacement part number of the PCI SA85 Modbus Plus card
Product Line:
Modbus Plus, 416NHM30030A, PCI SA85
Resolution:
The new part numbers for the PCI SA85 Modbus Plus network interface cards are:
Single Cable: Old number is 416NHM30030 and replacement is 416NHM30030A.
Dual Cable: Old number is 416NHM30032 and replacement is 416NHM30032A.
This card is an enhanced version of the older version of the card.
The new features are:
1. | The card will support the 3.3 and 5 volt PCI bus. |
2. | The card will now mechanically fit in the PCI-X server bus slots. However it is up to the motherboard manufacturer if it will support the 33 Mhz operation of this card. The PCI-X bus runs at the speed of the slowest device installed, these cards run at 33 Mhz. |
3. | The card will fit in both the PCI and PCI-X bus slots. |
4. | The MBX Driver Suite will recognize the card as the 416NHM3003x. The card is backwards compatible with the MBX version 4.2b driver suite. |
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: