{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to use an output contactor to open the motor circuit on the ATV12?

Issue: Is it possible to use an output contactor to open the motor circuit on the ATV12?

Product Line: ATV12

Environment: All

Cause: ATV12 and Output contactor

Resolution:
The ATV12 has been designed to support this kind of application without any particular precaution (without ferrite...).
So you can add an output contactor directly between the motor and the drive and open it even if the motor is loaded

Schneider Electric Egypt and North East Africa